Post Go back to editing

LT3798 18V 5A

Thread Summary

The user is designing a circuit with the LT3798 to achieve an 18V 5A output using the flight transformer 750811330. The final answer provides a link to a sample circuit for the required 18V 5A output, which can be used as a reference for modifications from the 24V 2A configuration.
AI Generated Content

Hi,

I am designing a circuit with LT3798, I need an 18V 5A output with the flight transformer 750811330. 

Can you tell me what I have to change with respect to 24V 2A

Thaks 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.