KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LT8357
Recommended for New Designs
The LT8357 is a wide input range, current mode, DC/DC controller which can be configured as a boost, SEPIC or flyback converter. The LT8357 drives a low...
Datasheet
LT8357 on Analog.com
Hi,
I want to develop a power supply circuit using the LT8357.
The output voltage is 5Vdc with a maximum output current of 2.5A.
The input voltage is always above 8V but during start-up it could drop to 3V for about 20msec.
So I was thinking of using the LT8357 in sepic configuration even if 99% of the time it will always work in buck mode.
Is there an excel to perform all the necessary calculations?
Regards
Robert