Hello,
I see that the peak current minimum value of ADP2107 is 2.6A. So for a GSM modem based application where the surge current is 2.15A for approx 0.5ms every 4.5ms, otherwise less than 0.8A.
In this case can an inductance value of say 2.7uH prevent peak current from hitting the 2.6A limit with (ΔIL/2 + Imaxload)?
So essentially the question is can a surge load described of 2.15A be handled by ADP2107?
Thanks, Prithvi