Post Go back to editing

high voltage High-side MOSFET output protection

Hi,

We are looking for a part suggestion that can help us implement the following.   I am hoping for a part that we can run up at 300V that drives an external MOSFET.  The part would have current sense and MOSFET driver.  The only problem is that the source voltage at the external mosfet can vary by 360V.

  1. Using a high-side N-channel MOSFET to provide the following functions:

1.a. High-side switch

1.b. When switching from off-to-on to provide an in-rush control to the load.

1.c. Protection of the output.  If current exceeds a value the output is switched from on-to-off immediately preserving the high-side MOSFET.

  1. The voltage input voltage is 300-360VDC nominally.  The output to the load is approximately the same voltage.
  2. The maximum output power is 400W approx..
  3. The circuit must provide:

4.a. in-rush limiting or voltage slew rate limiting.   Just someway to limit the voltage rise and current to the load when the MOSFET switches from off-to-on.

4.b. MOSFET when switched full-on must be able to deliver 2.5A nominally.

4.c. If there is a short at the output, the MOSFET must turn-off quickly enough such that the MOSFET can survive. 

4.d.  During MOSFET off-to-on during the in-rush to the load; this must also survive a short condition during that time.

  1. During a short condition of the output the MOSFET-source would be very close to zero voltage and so the MOSFET will be dropping 360V during that event approximately.    So whatever part we would select it would need some flexibility in the gate drive.  
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.