Hi
I am considering ADP1706.
I can start softly by attaching a capacitor to the SS pin,
What will happen if no capacitor is attached to the SS pin?
Will it be a soft start of about 48us like ADP1707 / 1708?
Best Regards
Yuya
ADP1706
Production
The ADP1706/ADP1707/ADP1708 are CMOS, low dropout linear regulators that operate from 2.5 V to 5.5 V and provide up to 1 A of output current. Using an...
Datasheet
ADP1706 on Analog.com
ADP1707
Production
The ADP1706 / ADP1707 / ADP1708 are CMOS, low dropout linear regulators that operate from 2.5 V to 5.5 V and provide up to 1 A of output current. Using...
Datasheet
ADP1707 on Analog.com
Hi
I am considering ADP1706.
I can start softly by attaching a capacitor to the SS pin,
What will happen if no capacitor is attached to the SS pin?
Will it be a soft start of about 48us like ADP1707 / 1708?
Best Regards
Yuya
Hi Yuya,
The soft start of ADP1706 without a soft start cap will be similar to that of ADP1707 and APD1708, which is 100us.
Regards,
Bryan
Hi Yuya,
The soft start of ADP1706 without a soft start cap will be similar to that of ADP1707 and APD1708, which is 100us.
Regards,
Bryan