Post Go back to editing

Using ADI's LTC7806 in sync mode Question?

1. Whether or not BURST MODE can be driven when using in synchronization mode.

I am trying to use it in synchronization mode by connecting MASTER PIN12(CLKOUT) -> SLAVE PIN25(PLLIN/SPREAD). When synchronizing, there is a message below that the operation mode is changed. Do I need to use a specific mode for synchronization? Currently configured in burst mode. (PIN4 connected to GND)

2. Whether SLAVE BOOST IC ON/OFF can be implemented.

I want to turn on/off the SLAVE IC as needed. Can I use it by turning ON/OFF using a switch on PIN5 (RUN)? Is there any damage due to the MASTER output when SLAVE OFF?