Hello,
I have one question about Vout range for LTC7149.
In LTC7149 datasheet, the output range is shown as 0V to -28V in page 1 Features,
and the absolute maximum rating for GND pin reference to Vout- is also 28V max.
But in LTC7149 EVB DC2354A manual, it claimed that output could be as low as -60V.
The 'User Select' option is just a jumper connect to a resistor slot.
I've checked Vout-/VoutSNS/GND and related circuit in DC2354A schematic,
but I can't find any level-shift or attenuate design that may help with GND-to-Vout- limit.
Did I miss anything ?