Post Go back to editing

LTC2980 VPWR Unexpected Voltage drop on input

Hello, I have an LTC2980 Power Sequencer with the input power connected similarly to shown in Figure 30 of the LTC2977 datasheet.

The difference is that I have a Schottky Diode between the system 5V and the LTC2980 VPWR inputs.

I am seeing a 1V drop across the Schottky Diode that I'm not expecting.  In other words the VPWR inputs are measuring 4.0V. 

This tells me that the current draw on these pins (A_VPWR and B_VPWR) are many Amps.

Any ideas why I would be seeing this voltage drop?  Thanks.

Edit Notes

Corrected part numbers.
[edited by: ja424fs at 8:49 PM (GMT -5) on 10 Feb 2022]
Parents
  • First, let me ask why you need to add a schottky to VPWR.  The VPWR pins may go to GND while VDD33 is applied.  That is, there is no internal diode between VDD33 and VPWR.  An external diode is not necessary.

    A BAS70 is rated for 70mA max. It may fail open or resistive if it sees high current.

    The 2980 has two 2977s inside, and the pinout allows you to treat each 2977 as a separate chip.  Have you tied the two VPWR pins together?  Each 2977 draws ~10mA, so 20mA total.  If the schottky is dropping 1V, then it will be obvious whether the 2980 is drawing lots of current by feeling the package to see if it gets hot. 

    Did you leave the DNC pins floating?  

    Regards

    Mike

  • I don't know why the Schottky diode is there as I "inherited" the design.  There may have been some concern that current would pass through the LTC2980 when powered by VDD33 for programming.

    • The A_VPWR and B_VPWR pins are tied togther.
    • The Schottky diode is not hot.
    • The A_DNC and B_DNC pins are floating.
  • OK, I see.  The purpose of the PFET is to shut off when Vin is applied, the gate pulls high.  This allows the internal 3.3V LDO to operate.  If Vin is 5V, I suggest removing the gate divider and tie the gate directly to VPWR/5V.  We added the divider to the datasheet since most apps use 12V for Vin and some PFETs in the past had 8V limit to Vgs.  When Vin is powered off, the gate goes to GND, and the PFET is fully on, connecting the external 3.3V supply to VDD33.

    I suggest you replace the diode with a zero ohm SMD jumper.

    Mike

Reply
  • OK, I see.  The purpose of the PFET is to shut off when Vin is applied, the gate pulls high.  This allows the internal 3.3V LDO to operate.  If Vin is 5V, I suggest removing the gate divider and tie the gate directly to VPWR/5V.  We added the divider to the datasheet since most apps use 12V for Vin and some PFETs in the past had 8V limit to Vgs.  When Vin is powered off, the gate goes to GND, and the PFET is fully on, connecting the external 3.3V supply to VDD33.

    I suggest you replace the diode with a zero ohm SMD jumper.

    Mike

Children