Post Go back to editing

LTM8002HY Schematics design help

Hi all!

I would like to use the LTM8002HY in my design.

The design specs are:

Vin = 5V

Vout = 3.85V

Iout = 1.5A

* The load during startup is only 0.5A and only later the 1.5A is needed.

Can the LTM8002HY fit my design specs? is there enough voltage difference? which Fsw is best and what other values i should keep an eye on when designing my schematics?

Thanks,

Ido