Post Go back to editing

Question about LTM4601

I have a question about LTM4601.

I am using LTM4601 and checking fSET pin voltage on DMM, and it is 7.7V. 

However, the fSET absolute range on the datasheet is "–0.3V to INTVCC + 0.3V".

It means that 7.7V violates the absolute range.

Please tell me if 7.7 voltage is expected figure or not? Is it a typo on the datasheet?

One more information,  at page 21 on the datasheet, it says s. The fSET pin voltage is 1/3 of VIN.

I use VIN as 24V, so I believe   fSET should  be about 7V.

Thanks,

Tarzan2