Hello,
I am designing Boost convertor with below specs.
Vin DC : 4V to 24V
Vout DC : 24V regulated, 150mA
Efficeincy : >80%
I tried simulation using LT8570-1 as attached. Reference is taken from device datasheLT8570_DC2297A-A_TA02A (1).ascet itself. But circuit is giving initial oscillation & then stable output at 12V. Is there any issue in simulation file as it not generating 24V output.
Thanks in advance.
Praful