Hi all,
Our company is looking to use the LT3478-1 device and we wanted to confirm if there is a known problem with the device becoming unstable at a given point as per these previous topics:
RE: LT3478-1 Pulsates Under Some Circumstances
In both cases the pulsing was said to occur around 14-15Hz. We are simulating the system as per the recommended LTspice simulation and have not observed this. We only have made two small changes:
1. Removing the MOSFET since we don't need PWM dimming
2. Increasing the input voltage to 25V and connecting our LED string which draws 0.2A at 40V.