Hi,
Our design uses LTC4212 for 3.3V ORing.
Current Rating: 4A (max)
Following MOSFET has been chosen for the design: Si6423ADQ / Vishay
Pl let us know if this MOSFET is good enough for the application?
Best Regards,
Pons
LTC4412
Recommended for New Designs
The LTC4412 controls an external P-channel MOSFET to create a near ideal diode function for power switchover or load sharing. This permits highly efficient...
Datasheet
LTC4412 on Analog.com
LTC4212
Production
The LTC4212 is a Hot Swap™ controller that allows a board to be safely inserted and removed from a live backplane. An internal high side switch driver...
Datasheet
LTC4212 on Analog.com
Hi,
Our design uses LTC4212 for 3.3V ORing.
Current Rating: 4A (max)
Following MOSFET has been chosen for the design: Si6423ADQ / Vishay
Pl let us know if this MOSFET is good enough for the application?
Best Regards,
Pons
Hi,
Are you sure that you have the right part numbers?
The LTC4212 is a Hot Swap controller that requires an N channel MOSFET.
The Si6423ADQ is a P Channel MOSFET
JayBee
Hi JayBee,
Apologies for the wrong PN. Correct PN is: LTC4412.
- Pons
Pons,
Based on this graph from the MOSFET datasheet:

And the RDSon, the Si6423adq is a suitable MOSFET.
The forward voltage drop of the ideal diode will be around 60mV.
JayBee
Thanks JayBee for the analysis & confirmation.
- Pons