Hi~~!
I have a problem.
I made a strobe light a long time ago using a DC1470A circuit with CBT-90-B.
The layout of the parts, traces, vias, etc. were copied almost as-is.
The parts are slightly different from the specifications presented. Value is the same.
For example, tantalum capacitors... (SONY => AVX)
However, FET, Inductor, and Diodes are exactly the same. (RJK0305, RJK0330, SI7234, WURTH 1.3uH)
I have been using it without problems for 7 years, but problems are coming out in this production.
Slowly increase the current to 20A and there is no problem.
However, 0,20A,0,20A..., when driven with a strobe like this, the current increases and then falls as shown in the attached figure 1.
About 15ea of the total 700ea productions occurred.
I know that CBOOT is involved.
However, the CBOOT Capacitor was 220nF from the beginning and has not changed for 7 years.
The problematic B/D was tested as follows.
(Only tested on each corresponding part.
V_in = 12V 10A Power Supply
PCB: 4 layers, 1oz (top, inner, bot)
- Replace R8,R7,C9,C10,C15,R15,R16 ... Still Fault.
- CBOOT Cap (220uF). Replaced with 330nF. It works normally. samsung mlcc
- C27(10uF) Cap. remove. It works normally. samsung mlcc
- Replaced Q1 (RJK0305). It works normally. It was supplied from an authorized RENESAS dealer.
- vcc_int normal 5.1v
- No abnormalities in parts related to Diodes, Inductor, Sense+, -, VCH, and VCL.
Are there any additional things to check?
Any comments would be appreciated.
Thank you. ^_^
For reference, the waveform for a normal product is as follows.