LT8364
Recommended for New Designs
The LT8364 is a current mode DC/DC converter with a 60V, 4A switch operating from a 2.8V to 60V input. With a unique single feedback pin architecture it...
Datasheet
LT8364 on Analog.com
Hi, ADI experts:
I want to convert a -12V input DC voltage to a -1.5V to -5.5V, Io=-3A output DC voltage by LT8364, is it possible?
my assumption is shown below. Any more detailed application circuits or notes could be given for LT8364, especially for the level shift circuit. thanks a lot!
Merry Christmas!