When V_TRK is 0V, ADP1707 has reverse current by external circuit.
In this case, ADP1707 has protection of reverse current?
Thank
ADP1707
Production
The ADP1706 / ADP1707 / ADP1708 are CMOS, low dropout linear regulators that operate from 2.5 V to 5.5 V and provide up to 1 A of output current. Using...
Datasheet
ADP1707 on Analog.com
When V_TRK is 0V, ADP1707 has reverse current by external circuit.
In this case, ADP1707 has protection of reverse current?
Thank
Hi Ryan,
ADP1707 does not have internal reverse current protection. It is recommended to add a diode from output to input to conduct this fault current you're expecting.
Best regards,
Bryan
Thank you
Thank you