Post Go back to editing

LT3743 : Current Difference between channels.

I use two LT3743 on one board.

When output 6A, the difference of channels is about 300mA.

CH-A is normal, CH-B is low current.

This phenomenon didnot occur on large boards, but this phenomenosn occurs on small boards( 1/4 size)

As a result of the test, it seems to be determined by the stage after the output mosfet.

drive.google.com/.../view

https://drive.google.com/file/d/1KJdcxujOw4950-dG5erYFg_IxdSYa-Fj/view?usp=sharing

(It is not a difference in Mosfet device. I tried intalling SWAP, but the result is the same)

 https://drive.google.com/file/d/1QBbIbor2TW7Pd0oxRX0zVmSpcIGH6zzt/view?usp=sharing



file add
[edited by: MrBogus at 4:44 AM (GMT -5) on 11 Dec 2021]