Hi,
I am using ADM1270ACPZ-R7 hotswap.
My requirement is to set current limit to 500mA.
So, from datasheet, I am using adjustable current limit formula.
I have used resister divider to set Viset to 800mV.
My Vsense is 20mV.
Iset =500mA.
At Foldback(FLB) pin i have used resister divider top resistor=100K, bottom resistor=3.16K.So, FLB voltage is 0.735V.
Using above set values, i am not able to get the output from Hotswap.
But when i use fixed Vsense to 50mV, My Iset is coming out as 1.25A and hotswap output able to get.
Could you please confirm if adjustable current limit can be set.
Please check if i am missing anything when adjustable current limit is configured.
Thanks & regards,
Reshma,
HCL Technologies,
India.