Post Go back to editing

LTC3855 Enable control issue

Thread Summary

The user is experiencing an issue with the RUN pin of the LTC3855IUJ#PBF going high (~4V) despite being pulled low by an external power sequencer. The support engineer suggested checking the connection between the power sequencer and the LTC3855, as well as ensuring the power sequencer is not biased from INTVCC. The user confirmed there is no connection between the RUN pin and the power sequencer, and INTVCC is not connected to the sequencer.
AI Generated Content

Hi,

I am using LTC3855IUJ#PBF as 10V to 6V buck regulator. we are using both the channels for same voltage generation.

Observed that when I applied 10V to VIN pin, RUN pin of regulator goes high ~4V even though pulled low from external power sequencer.

Parents Reply Children
No Data