Post Go back to editing

LTC4413 What happens if a voltage is applied to INB when ENBB is High?

Hi,

I have a question.
Please give me an answer.

About LTC4413,
If a charge is input to the INB while the ENBB is at the high level, the OUTB will be in the output state for a short time.

Is it normal operation?

・By the way, INA is 0V and ENBA is Low.

・ When INA and INB start up from the low state of ENBA and ENBB, the power is normally turned on (no short-time output).
・ If INA and INB are ON and ENBA and ENBB are set to High, they will be turned OFF normally. (No short-time output)

Best Regards,

Naohisa

Parents Reply Children
No Data