Post Go back to editing

DC590B Cannot Load Module for LTC4291 on DC2685B Eval Kit

After updating the QuikEval software and confirming connection to my unit (QuikEval comes up with the message "Found Device LTC4291 Click OPEN to begin"), the software will display a warning message "Cannot Load Module" when pressing the open button. I looked through the files and see that there is no ltc4291.ini file in the directory so that may be the issue. Can I have access to download the module directly? Thanks.

Edit Notes

Duplicate images. One deleted.
[edited by: KevinR at 10:16 PM (GMT -5) on 2 Dec 2021]
Parents Reply Children
No Data