Post Go back to editing

LT8304-1 dual outpu

Hello Team,

I have a requirement to generate +240V and -240V output from a single flyback controller with VIn=15V (20mA max o/p to power ADHV4702-1 extended volatge rail operation)

I have looked into the LT8304-1 datasheet, and hopefully looks it would be possible. An application note EVAL-ADHV4702-1CPZ User Guide provides a solution for +-110V voltage output using LT8304-1.

Can you suggest a suitable dual transformer for the application and whether this would be the right choice of the Flyback IC?