Post Go back to editing

LTC2953 with multiple sources

I want to use the LTC2953-1 in our project that requires the following function

1. When the wall-adapter power is connected, LTC2952 should AUTOMATICALLY enable the Output without needing to press the push-button driving the DC-DC

2. When the wall-adapter power is removed, LTC2952 should automatically revert to the connected battery to supply output

3. Turn on power when the push-button is pressed for more than 900ms

4. Turn off power when the push-button is pressed for more than 900ms

Is the LTC2952 the right part for these functionalities? 

Parents Reply Children