KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADM7150
Recommended for New Designs
The ADM7150 is a low dropout linear regulator that operates from 4.5 V to 16 V and provides up to 800 mA of output current. Using an advanced proprietary...
Datasheet
ADM7150 on Analog.com
Hello,
Is it possible to connect 5x ADM7150 in serie in order to reach 25V (output voltage) ?
Best regards,
I'm not familiar of application that put LDO's in series. Can you share more info about what you want to achieve?
I'd like to reach an output around 15v. I was thinking why not set the output of 3x adm7150 in serie. What do you think ?
You may consider choosing LDO with capable of higher voltage instead of configuring multiple LDO's in series which the said configuration is not widely used. You can select in the ADI selection table in analog.com:
Selection Table for LDO Linear Regulators | Parametric Search | Analog Devices
Regards,
Noel