Hi Sir,
I have some questions on LTC4364. The design schematic as below:
1) Input volatge=10.8V~52.8V
2) Input current= 50A @ Vin=10.8V
Input current= 10.3A @ Vin=52.8V
a. Do the PD1 and PD2 must for this design? The input of PJ1 connector don't need to support hot swap and the PJ1 has foolproof design.
b. If PD1 and PD2 must to added. What voltage rating need to use for the PD1 and PD2?

Edit Notes
Modify input rating[edited by: cnaon3264 at 4:16 AM (GMT -4) on 21 Oct 2021]