Hello,
Is there any LT3065 product which has a junction temperature of 175°C or higher? MP- and H- grades have a junction temperature of 150°C, are these absolute maximum values? What happens when the temperature exceeds 150°C? Asking this because in my project, I have a problem with high power dissipation. My values are:
Vin_max = 29.5V, Iload = 117mA, Vout = 5V, Tambient_max = 50°C
Can I use any LT3065 product if I have such values in my project?
Best regards,