Post Go back to editing

LT3761 Sync Option

Thread Summary

The user inquires about using two LT3761 drivers to replace an LT3797, focusing on the Sync pin functionality. The final answer confirms that if the Sync pin is not used, it should be connected to PWMOUT to prevent LED flicker and ensure good PWM dimming performance. The OPENLED pin can be tied to GND if not used, and this configuration is compatible with both LT3761 variants.
AI Generated Content

Looking to use TWO LT3761 drivers to replace the LT3797 we were currently using. I never used the "Sync" option and wasn't planning on it, but in the event that I do - How do I use the Sync pin to sync two of these together? The datasheet doesn't seem to give enough details on that. Is there an example schematic for such connections?

Also, if I don't use the Sync feature, the datasheet states to connect the pin to the PWM_OUT pin instead. Is this correct? The LT3755 states to connect it to GND.... If I procure the LT3761 that has the OPENLED pin, is there any harm by having that connected directly to the PWMOUT? I want to design this so I can use either LT3761 chips due to availability...

Thanks,