Post Go back to editing

ADM7151 Adjusting output voltage response time not consistent

Hi,  I have a board with ADM7151, and I adjust the output voltage with an additional resistor to the ref_sens pin going to a DAC as shown in LTspice schematic.

In the simulation, the output voltage responds to change in the DAC in a few milliseconds. However, then I measure the behavior on the board, I find that sometimes the output voltage takes seconds to rise. It only happens when setting a higher voltage, not a lower voltage. Additionally, it only happens when the difference in new output voltage to the current voltage is small, less than 0.4V.

I can not reproduce this behavior in the simulation, which is attached.

ADM7151_adj.asc



removed screenshot, was earlier version of ltspice model
[edited by: cdai at 5:53 PM (GMT -4) on 30 Sep 2021]
Parents
  • Hi Chenxi,

    What you're seeing is a byproduct of the low noise architecture of the LDO. Applying DAC to change voltage is valid but the delay in settling time is present. When you apply small changes on the REF_SENSE, that translates to a small differential voltage on the input of the OTA, and further translates to a small change in current on the OTA output (BYP; final stage of the reference voltage setting). This leads to large slew rate and high impedance on the BYP pin. 

    Regarding LTspice, since modelling targets normal mode operation or behavior, this occurrence is not modelled exactly due to limitations.

    Hope this helps.

    Regards,

    Bryan

Reply
  • Hi Chenxi,

    What you're seeing is a byproduct of the low noise architecture of the LDO. Applying DAC to change voltage is valid but the delay in settling time is present. When you apply small changes on the REF_SENSE, that translates to a small differential voltage on the input of the OTA, and further translates to a small change in current on the OTA output (BYP; final stage of the reference voltage setting). This leads to large slew rate and high impedance on the BYP pin. 

    Regarding LTspice, since modelling targets normal mode operation or behavior, this occurrence is not modelled exactly due to limitations.

    Hope this helps.

    Regards,

    Bryan

Children