LT8471 Flyback 2-pair output ref circuit

I wanna use one IC to output 2-pair output by flyback circuit.

LT8471 is the only one that has two output and two voltage control pin(FB1&FB2). But there's no flyback circuit to refer in LT8471 website.

I wanna use 1to2 transformer(like Sumida CEP1311E) and FB1&FB2 to change my output voltage. So I use LT8471's LTspice model to draw an abnormal circuit as below.

I'd like to know how to correct the circuit to have a 2-pair output(VPP_1/VNN_1 and VPP_2/VNN_2) circuit.

Thanks.

Parents Reply
  • I checked LT8302, it's familiar with LT8304, but there's no ref pin for LT8471 to use.

    LT8331 has flyback demo circuit, I try to follow the flyback circuit and draw a circuit as below.

    From LT8471's spec I got the Vout formula. Vout=VFB*(Ra/Rb+1), and Vout = Vfw_1 in the circuit.

    And then secondary side voltage formula comes from LT8331 as below. 

    From LTspice simulation result VPP=215V, it's seems right when R8=400k, R7=10k, D=0.4. But how can I know D? or how to estimate D?

    Thanks.

Children