Post Go back to editing

ADP2503 - Over Current consumption

HI,

Hope you are doing well!

Please find the below query regarding : ADP2503ACPZ-3.3-R7 IC 

1. We are operating in Forced PWM mode , then the current consumption is as given below:

a) at 3.3V input : 9mA is current consumption

b) at 3V input: 9mA is current consumption

c) at 4.2V input : 6mA is current consumption

we are operating at fixed output voltage mode : 3.3V output

Can you suggest me on the reason why it's consuming more current or suggest ways to reduce current consumption

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.