HI,
Hope you are doing well!
Please find the below query regarding : ADP2503ACPZ-3.3-R7 IC
1. We are operating in Forced PWM mode , then the current consumption is as given below:
a) at 3.3V input : 9mA is current consumption
b) at 3V input: 9mA is current consumption
c) at 4.2V input : 6mA is current consumption
we are operating at fixed output voltage mode : 3.3V output
Can you suggest me on the reason why it's consuming more current or suggest ways to reduce current consumption