Post Go back to editing

LT8616 Voltage in VOUT1 is unable to regulate to 5V and outputs 11V; power good 0V for VOUT1

Hello,

I have used LT8616 in my recent project and expected everything to work fine but the chip outputs 11V instead of 5V. This fired almost the entire system.

Input 12V,

Output 1: 5V(expected) 11V (actual) Output 2 :3V3

PG 1 : 0V PG2: 3V

I will attach the snippet of the schematic for reference and your inputs.

Thank you 

GPS

Parents Reply Children
No Data