The user manuals state the max Vin is 18V for both dev kits. Is there a way to increase the max Vin? Why is the set to 18V since the LT8253 has a max Vin of 40V?
manuals
Obsolete
manuals on Analog.com
LT8253
Recommended for New Designs
The LT8253/LT8253A are synchronous 4-switch buck-boost controllers optimized for automotive USB-C power delivery. The LT8253/LT8253A are fully compliant...
Datasheet
LT8253 on Analog.com
The user manuals state the max Vin is 18V for both dev kits. Is there a way to increase the max Vin? Why is the set to 18V since the LT8253 has a max Vin of 40V?
Hi Tom,
This is just a limit in the firmware for the USB port controller and can be reconfigured. This application was centered around automotive input voltage range, but can tolerate higher input voltages.