Hi,
I am using the product LTC3877 & LTC3874 to generate a four phase core supply for the Arria10 GX FPGA . The design I have used is the same as in the Arria10 GX FPGA Development Kit schematics. However I require a few clarifications.
We are providing a 12V input to generate 0.9V core Voltage Supply (85A) .
What is the current limit set in the LTC3877 with 15mV Voltage on the ILIM pin .
As per the LTC3874, the Current limit programming should match with the LTC3877 (Master controller). However in the reference design the LTC3877 is 1/4 of INTVCC(ILIM pin connected to voltage divider) and the LTC3874 is connected to GND. Is this ok .
Also we are unable get LTC3877 part in LT power cad tool.
Kindly clarify at earliest.
Thanks,
Aravind D