Post Go back to editing

LT8300 / LT8303 switching frequency

Thread Summary

The user asked for the formula to calculate the switching frequency of the LT8300 or LT8303 Flyback controllers based on load current, input voltage, output voltage, primary inductance, and transformer turns ratio. The final answer stated that the formula is not meant to be shared externally and advised using the graph provided in the LT8303 datasheet.
AI Generated Content

Hi,

Can you provide the mathematical formula allowing to calculate the actual switching frequency of the LT8300 or LT8303 Flyback controllers, depending on the load current, input voltage and output voltage (with parameters as primary inductance, transformer turns ratio, etc ...). The LT8303 datasheet provides the example with Vout = 5V (refer here-below), my query is to be able to calculate the same curves with all the parameters.

Many thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.