Post Go back to editing

LTC2995/2994

We are planning to use either LTC2995 or LTC2994 push button controller in our design.

After going through the datasheets of both the parts, the parts are meeting our requirements except following points regarding debounce time for ON and OFF.

LTC2995:

  1. There is no option for programming the debouncing time for ON event. Only the default option of 32ms is available.
  2. There is no option for programming the debouncing time for normal OFF event (not the force OFF through TMR pin). Only the default option of 32ms is available.

Is there any way to add larger debounce time in the range of seconds for ON and OFF events?. It is preferred to have more debouncing time for OFF than ON.

 

LTC2994:

  1. There is an option for programming the debouncing time for ON event.
  2. But there is no option for programming the debouncing time for normal OFF event (not the force OFF through TMR pin). Only the default option of 32ms is available.

Is there any way to add debounce time for OFF event. It is preferred to have more debouncing time for OFF than ON.

Regards,

Saravana

  • Hi Saravana.
    I believe you mean the LTC2954 and LTC2955 pushbutton controllers.


    If you want adjustable on and off timers, the LTC2954 is best for your application.

    Is there any way to add debounce time for OFF event. It is preferred to have more debouncing time for OFF than ON.

    For power down via the PB# pin, the LTC2954 has 64ms of debounce by default, but additional delay can be added via a capacitor on the PDT pin. See page 9 of the datasheet for the equation to calculate the value of CPDT , given your desired delay.

    -Aaron

  • Dear Aaron,

    Thanks for your response.

    We are planning to use LTC2955 due to our requirements. If I add an external RC debouncing on PB pin, will there be any impact in LTC2955 operation? I have attached a reference circuit for having around 600ms of debouncing for ON and OFF.

    Please check and confirm.

    Regards,

    Saravana

  • Hi Saravana,
    I built your circuit in LTSpice (sim file attached).
    2955-1 EZ debounce 9-3-21.asc

    As is, it doesn't work.
    It's because the PB# pin doesn't discharge to 0V when the switch is pressed.
    This is because there is an internal pull-up to an LDO that needs to be factored in.

    When considering the internal pull-up, the cap on the PB# should discharge to ~820mV.
    Coincidentally, the typical threshold for the PB# pin is 800mV.
    There isn't enough margin; PB# must go below 600mV when the switch is pressed (the minimum threshold possible).

    When I lowered the 200k resistor to 100k, I was able to get the EN pin to change state.

    I will leave the sim file with you to determine what the right RC values are.

    -Aaron

  • Hi Aaron,

    Thanks for your quick response.

    I understand the concern stated by you.

    I have requested my IT colleague for installation of LT Spice in my machine.

    I will check and get back for any further information.

    Regards,
    Saravana

  • Hi Aaron,

    I have an additional question regarding KILL input. As per my understanding from datasheet, always KILL input is related to PB input and INT output pins. Is it possible to control the KILL input by uP or any other peripheral independent on PB input pin? 

    Regards,

    Saravana

  • Hi Saravana,
    Yes, that is possible.

    From the datasheet’s pin description: “A low at KILL# releases the enable output (EN/EN). This pin can be driven by the microprocessor or it can be used as a voltage monitor input.”

    KILL# is independent of PB# and INT#.

    Be aware of the KILL blanking time, where the KILL# input is ignored for 512ms after EN goes high.

    -Aaron

  • Hi Aaron,

    Thanks for quick response. That was helpful.

    We have a query regarding figure shown for "Power First Applied to LTC2955-1" (Ref: Figure-7 in datasheet).

    We are not using ON pin and hence grounded in design. So we would like to understand the "Power First Applied to LTC2955-1" without consideration of ON pin relation. A sequence with only VIN, PB Pin and EN Pin is what we are looking for. Or we would like to know the status of EN pin during first power application. Please check and let us know your inputs.

    Regards,

    Saravana

  • we would like to know the status of EN pin during first power application.

    EN starts off LOW.

    we would like to understand the "Power First Applied to LTC2955-1" without consideration of ON pin relation. A sequence with only VIN, PB Pin and EN Pin is what we are looking for.

    I ran a simulation to show the timing diagram of these pins. See the pic below.

    At t=1sec, IN steps from 0V to 6V

    Note that there is a 1s lockout time (typ) after VIN reaches UVLO of 1.15V. PB# inputs are ignored in this window, so I wait 1.5s to be safe.

    At t=2.5s, PB# steps from 1V to 0V. (Falling edge)

    At t=2.5313s (~32ms later), EN goes high.

    Note that there is a 512ms KILL blanking time after EN goes HIGH, where PB# inputs are ignored.

    At t=4s, PB# steps from 1V to 0V. (Falling edge)

    At t=4.1103s (~110ms later), EN goes low. This is close to the calculated 116ms of debounce off time.

    Here is the sim file:
    2955-1 EZ 9-22-21.asc

    -Aaron

  • Hi Aaron,

    Thanks for quick response.

    After seeing the waveform I got a doubt regarding TMR capacitor. Actually it will add extra debounce only for force KILL option rigth in case of software fails to control the KILL input? Otherwise the normal debounce time will be 64ms and shutdown will happen through INT and KILL pins. Is this understanding correct?

    Regards,

    Saravana

  • Yes, I believe your statement is correct.

    I encourage you to download LTspice and play around with your circuit.
    This will let you check if the part works as you expect.

    Have a good day,
    -Aaron

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.