Hi,
we run into Problems when using the LTC7001 for a Brushed Motor Control. We want control the Input Pin with a 20kHz PWM Signal. We have this Circuit:
I already added the TVS Diode from GND to Ts Pin.
The Problem:
The FET has a Qg from 75nC so for PWM i decided to use 100nF Boost Capacitor. But The Gate Voltage will only go up to Ts + 5V.
Then i changed the Boost Capacitor to 1uF now i will have a Gate Voltage of Ts + 12V but with 80% PWM the Driver Stops after some seconds working, will pause a second and remain working. I can't figure out why the driver is stopping.
Can somebody explain this? OV and UV are at Max and Min values. I don't see any Voltage drop on VCC.
Thank you,
Florian