Hi,
Is LT8471 suitable for below configuration?
Vin= 48V
Vout 1=33V (2A)
Vout 2=3.3V (0.5A)
LT8471
Recommended for New Designs
The LT8471 is a dual PWM DC/DC converter containing two internal 2A, 50V switches and an additional 500mA switch to facilitate step-down and inverting...
Datasheet
LT8471 on Analog.com
Hi,
Is LT8471 suitable for below configuration?
Vin= 48V
Vout 1=33V (2A)
Vout 2=3.3V (0.5A)
Hi jiamin,
I think you need to do sepic on channel 1 then buck on channel 2. Please check this as option: LT3992 dual converter.