| SLA Status | Assignee | Support Status |
|---|---|---|
| ⚠ 4557 hours | Open | |
ADP5092
Production
The ADP5091/ADP5092 are intelligent, integrated energy harvesting, ultralow power management unit (PMU) solutions that convert dc power from PV cells or...
Datasheet
ADP5092 on Analog.com
A few questions with respect to the ADP509x devices.
1. The ADP509x data sheet states in a couple of places that "for the best operation of the system, use PGOOD to enable the system load or to turn on an ultralow power load PFET". Exactly what performance benefit is achieved by using an additional external load switch?
2. If SYS or Reg_Out are enabled via an external load switch using PGOOD or REG_GOOD (5092 only), power to a connected load will experience a rather fast leading edge. Connected load capacitance will likely result in currents exceeding device limits, 1000 mA for SYS and only 150 mA for Reg_Out. Reg_Out is described as having an internal current limit of ~200 mA and SYS is stated as having no internal limit. It is further recommended to limit SYS and BAT currents to less than the 1000 mA spec. My questions are primarily associated with the Reg_Out piin as that is the pin I plan on using.
Thanks much for any clarification you can provide.
stephenv - Moved from Other Products (EN) to Power Management. Post date updated from Thursday, August 12, 2021 6:02 PM UTC to Tuesday, February 3, 2026 9:06 PM UTC to reflect the move.
stephenv - Moved from Other Products (EN) to Power Management. Post date updated from Tuesday, February 3, 2026 9:06 PM UTC to Tuesday, February 3, 2026 9:06 PM UTC to reflect the move.
Hi,
1. with the PGOOD, it can make sure the BAT is connected to the system and the hysteresis can also help the support the startup current of the system.
2. For SYS, you can use an external load switch and there is a capacitor at SYS pin so it should be fine for the startup current. For REG_OUT, there are REG_D0 and REGD1 as the enable pin so you don't need extra load switch. The REG_OUT pin cannot support 800-1000mA startup current. The current limit is 260mA typically.
Can you clarify where this high surge current is from?
BRs,
Kevin
I am assuming there is some voltage level present internally at the internal regulator output when the internal REG_SWITCHES switch on that would lead to a fairly fast output rise, ie. a step output to this level. Waveforms in the data sheet seem to indicate this, though after a more careful look, this rate of rise may not be as fast as I was first thinking. If Vsys (BAT) however is up to some charge level and Vsys is enabled via an external load switch, the output of the load switch would be a step rise to the Vsys level present when PGOOD goes active. Applying a voltage step to any significant load capacitance would lead to a high capacitive in rush current.
Similar in rush levels might occur if portions of external loads are turned off, essentially disconnected, and later reconnected. In this case, a fully discharged load would be re-connected to the full output of the power rail supplied by the ADP509x, and any load capacitance would again be subjected to a step voltage input. This could occur at either the SYS or Reg_Out outputs.
I am concerned over time that these turn on current spikes, either when the ADP509x outputs are enabled directly, through an external load switch or an external load comes in and out of different sleep modes might harm the ADP509x outputs.