Post Go back to editing

LT3092 bypassing minimum current

Hey,

Is it possible to bypass the minimum current of 0.5mA of the LT3092 to avoid it to go trough the load?. Specially for the case when the load is near to 0Ohms.

  • Hello,

    the LT3092 does see only 'one' load for his pins where he sources the minimum of 0.5mA.

    If you want to separate the output current into two 'streams', one for the minimum output current of 500uA and one for your 'real' load I would suggest to use another LT3092 in parallel to your load which will be configured for your minimum load as well. So you have a stack of two 3092 where the lower LT3092 is working in parallel to your load.

    Do you have enough voltage headroom to do so?

    kr

    Markus

  • Hey MarkusHP,

    sorry for the late answer. I think another LT3092 in parallel to the load wouldn't work when the output Voltage of the 'upper' LT3092 is lower then 2V.

    Any other suggestions?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.