Post Go back to editing

LT3932 ISMON accuracy

Hello,

we would like to use the current monitor output ISMON in order to save a dedicated OPamp circuitry or current sense monitor IC for an application where we use max. 2:1 analog dimming via ctrl input . This means the current sense amplifier will have a sense voltage between 50mV and 100mV. The datasheet specifies:

ISMON Voltage VISP - VISN = 100mV (100%), VISP = 12V
V
ISP - VISN = 10mV (10%), VISP = 12V
0.965 1.000 1.030
80      100     120
V
mV

So approx. +/-3.5% for 100mV and +/-20% for 10mV sense voltage across VISP and VISN for Ta = 25°C. What accuracy can we expect for 50mV sense voltage over full operating temperature range (-40°C to 85°C) ? If you can provide a graph or similar, this would also help. Thanks in advance!

Regards Andreas

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.