KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LTM4653
Recommended for New Designs
The LTM4653 is an ultralow noise 58V, 4A DC/DC stepdown μModule® regulator designed to meet the radiated emissions requirements of EN55022. Conducted...
Datasheet
LTM4653 on Analog.com
LTM4630A
Recommended for New Designs
The LTM4630A is a dual 18A or single 36A output switching
mode step-down DC/DC µModule® (micromodule)
regulator with wider VOUT range and higher efficiency...
Datasheet
LTM4630A on Analog.com
Hello,
My customer will use LTM4653 and LTM4630A and before applying these devices, they want to confirm simulation results from LTSPICE.
But they say that the simulation time of their design takes long time, so they want to use a Loop Compensation Design (DCDC modeling) for reducing simulation time.

【LT - Loop Compensation Basics Buck Converter CCM】
In case of LTM4630A, when they use this modeling design, they got a similar results with stability value of Loop Comp. tap in LTPower Cad.
But in case of LTM4653, they have some problems to do the modelling desing and they can;t get right vlues.
Q) Would you confirm attached modeling file of LTM4653 and let me know your opinions?
For your reference, I also attached LTM4630A modelling files.
Please advise me.
Regards,
Sewoong
Except for phase at 100Hz, the results are very close, and 100Hz phase is not a concern.
The phase variance at high frequency is likely because the LTspice model is linear and does not account for the effects of approaching the switching frequency.
The phase variance at high frequency is likely because the LTspice model is linear and does not account for the effects of approaching the switching frequency.
Dear dkb,
Thank you for your reply.
But I have some questions about your answers.
Actually my customer's request get similar values both a result value of bode plot and stability value of Loop comp tap in LTPower Cad.
This is for using DCDC modeling file instead of LTSpice simulation at testing with various environments,
So they request your opinions about DCDC modeling files and LTPowerCAD files.
And also they say that DCDC modeling of LTM4653 is hard to implement because LTM4653 has different architecture from general DCDC like LTM4630.
So they want to get your advices about a DCDC modeling methods of LTM4653.
Q1) Would you let me know your opinions about a DCDC modeling file of LTM4630 that I attached?
Q2) Would you let me know your opinions about a DCDC modeling file of LTM4653 that I attached?
Q3) Would you explain how to implement a DCDC modeling file of LTM4653 in detail?
Q4) About your answers, is your answers about DCDC modeling file of LTM4653?
They want to get similar values between DCDC modeling file and LTPowerCAD file.
The standard is a LTPowerCAD and they want to meet values of DCDC modeling file to LTPowerCAD file.
Regards,
Se-woong