ADP5071 - Design tool - Runtime error 5

Hello

I have designed a power supply with the ADP5071 which works pretty good. Initial design is for 12V input, +/- 6V output. With LDO I have a very nice +/- 5V PSU. I managed to use the ADP5071 spreadsheet to calculate the design which was perfect. I have now tried to re-calculate do generate +/-13V. Unfortunately, I get always an error "Runttime error '5'" when I run the calculation. In fact the results seem no correct if I do a manual calculation for some components. I have tried almos everything with regards to security and langaue setting in Excel. I believe that the design tool has an issue with Office 365 and/or Windows 10.

Any Ideas ho to get is solved?

Thank you

Andy  

Parents
  • Hi Andy,

    I am currently using the design tool, and I have no problem using it with your input and output parameters (both +/-6V and +/-13V output). Can I know what are your other design parameters with 12Vin and +/-13V output?

    I'm currently using Windows 10 and Office 365 for the excel.

  • Hello Dave

    thank you for your answer. I'm in Switzerland, therefore I had to change my settings to English (US) but I still could not get the Speadsheet to work. 

    What I try to design is the following:

    Input voltage range: +9V ... +12V

    Output: +/- 13V, 330mA

    Switching Frequency: 1.2MHz or 2.4MHz (depending what the tool returns for the inductors)

    With L/C filter at the output (second stage filter)

    Vout Ripple: 0.6%

    Design Criteria: Most Efficient

    Thank you for your suppport!

    Best regards

    Andy

  • Hi Andy,

    Attached here is the Design tool with input parameters you have provided.

    Please let me know if you can change the individual components (inductors, output cap, etc.)

    ADP507x_Designer_Release.zip

    Regards,

    Dave

  • Hello Dave

    thank you for your support. I can open the file but not modify anything. As soon as I want to change a component or a design parameter, I get the run time error 5 message. I assume the problem is either related to the security seetings or to the language/region settings. Maybe I will install a computer with a US Windows 10 version and try to run it on such a machine.  

    Thank you and best regards

    Andy

  • Hello Dave

    I changed the region and language of my computer to English/US. There is still some strange behaviour when inputing the output current (issue with comma resp. point for decimal) but the calculation works.

    Thank you again and best regards

    Andy   

Reply Children
No Data