Post Go back to editing

ADP5090 Energy Storage Element Parameters

Hi team, 

Want to clarify  if the cold start power in requirement calculations of 33mW is accurate (based on ADP5090 calculation).

Is Capacitance requested is 12mF for this application? 

State V_sys_load (V) I_sys_load(mA) Period (s) V_batt (V) V_sys_bat_term (V) Converter Efficiency (%) Cin (mF)
Sleep 3.300 0.008 30.000 3.300 2.000 100.000 10.914
TX 3.300 4.000 0.010 3.300 2.000 100.000 1.819
Boot 3.300 1.230 0.200 3.300 2.000 100.000 11.187


Add on Energy Harvester Element Parameters table.
[edited by: John pg at 7:09 AM (GMT -4) on 22 Jul 2021]
Parents Reply Children