ADP1850, ADP1877 and ADP1829 are all dual channel buck regulator controllers. What are some of the key differences between these three?
ADP1850
Production
The ADP1850 is a configurable dual output or two-phase, single
output dc-to-dc synchronous buck controller capable of running
from commonly used 3.3 V...
Datasheet
ADP1850 on Analog.com
ADP1877
Not Recommended for New Designs
The ADP1877 is a Flexmode® (proprietary architecture of Analog Devices, Inc.), dual-channel, step-down switching controller with integrated drivers that...
Datasheet
ADP1877 on Analog.com
ADP1829
Production
The ADP1829 is a versatile, dual, interleaved, synchronous
PWM buck controller that generates two independent output rails from an input of 3.0 V to 20...
Datasheet
ADP1829 on Analog.com
ADP1850, ADP1877 and ADP1829 are all dual channel buck regulator controllers. What are some of the key differences between these three?