Post Go back to editing

Switching Regulators vs LDOs

Is efficiency the only advantage of switching regulators over LDOs?

  • The primary reason for selecting a switching regulator is efficiency; but at high current/power levels, size and cooling becomes an issue for linear regulators.

    Let’s compare an example of using a switcher versus a linear regulator to produce a 3.3V output at 3A from a 12V input.  The linear regulator will dissipate a lot of power with a 3A load, Pd = (12V-3.3V) x 3A = 26.1W.  This will require a large, finned heatsink to dissipate the heat, probably around 6” x 6” x 1” which is too large to be mounted on a PCB.

    In contrast, a switching regulator with 90% efficiency at a 3A load will dissipate, Pd = (3.3V x 3A)/(1-0.9) = ~1W which may be cooled by the surrounding PCB copper or just a small heatsink.  So the tradeoff between switchers and linear regulators is really efficiency and size.

    Also, linear regulators are generally cheaper and easier to implement.

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.