Post Go back to editing

On LT3085 typical app combo: hi-current with hi-efficiency

Thread Summary

The user inquired about combining a single LT3085 with a PNP amplifier to achieve higher current output, similar to the 5A output in the parallel LT3085 application. The final answer confirmed that this is technically possible but noted that the LTC3414 buck chip is limited to 4A output. The user then clarified their intention to use a Silent Switcher series buck solution, such as the LT8648, for the application.
AI Generated Content

Hi,

In the datasheet of LT3085, here are 2 typical application circuits.

Page 17:

Page 22:

So can they be a conbination? Namely, employ one LT3085 chip plus PNP amplifier, instead of four LT3085 chips parallel. To accomplish a higher current output. Here please despite whether the buck chip is able to afford a 5A load or ot.

Thanks a lot.

Highest Regards.

Jeronym Law