Post Go back to editing

ADSP-2148x E-pad question

Hello

I have just finished reading the EE- 352 Engineering note regarding E-pad packages and mounting techniques. One thing I am not clear of is you don't say whether or not you use thermal relief's or direct connects on the ground plane connecting via's. Obviously direct connection would give you better electrical connection and lower thermal resistance to the ground plane but would it alter the temperature profile needed for reflow ? ie which would be better from the point of view of manufacturability ?

regards

david

Parents
  • Pedro was confusing low resistance with "short"

    The impedance between Vint and GND will be low since this is where all nearly all the current draw will be.

    If the part was drawing 500mA, which is not actually the case at reset, etc, then 1.1V/500mA = 2.2 ohm

    Al Clark

    www.danvillesignal.com

Reply
  • Pedro was confusing low resistance with "short"

    The impedance between Vint and GND will be low since this is where all nearly all the current draw will be.

    If the part was drawing 500mA, which is not actually the case at reset, etc, then 1.1V/500mA = 2.2 ohm

    Al Clark

    www.danvillesignal.com

Children
No Data