Post Go back to editing

ADSP-2148x E-pad question

Hello

I have just finished reading the EE- 352 Engineering note regarding E-pad packages and mounting techniques. One thing I am not clear of is you don't say whether or not you use thermal relief's or direct connects on the ground plane connecting via's. Obviously direct connection would give you better electrical connection and lower thermal resistance to the ground plane but would it alter the temperature profile needed for reflow ? ie which would be better from the point of view of manufacturability ?

regards

david

Parents
  • Hello,

    I have designed my custom board with a ADSP-21489 (176 lead package) and I am having a problem with EPAD. After solder it on my board I was checking for short circuits and i found one between GND and VDD_INT (internal supply for ADSP). I removed the DSP and check the short circuit again and no problems found. Then I solder back the DSP and the short circuit is back.

    Since I have 2 DSPs I decide to check the connection between EPAD and GND. I verified something strange. The EPAD seems to be connected to VDD_INT pins and have no connection to GND pins. Is it normal?

    ADSP datasheet says that EPAD must be connected to GND.

    Best Regards,

    Pedro

Reply
  • Hello,

    I have designed my custom board with a ADSP-21489 (176 lead package) and I am having a problem with EPAD. After solder it on my board I was checking for short circuits and i found one between GND and VDD_INT (internal supply for ADSP). I removed the DSP and check the short circuit again and no problems found. Then I solder back the DSP and the short circuit is back.

    Since I have 2 DSPs I decide to check the connection between EPAD and GND. I verified something strange. The EPAD seems to be connected to VDD_INT pins and have no connection to GND pins. Is it normal?

    ADSP datasheet says that EPAD must be connected to GND.

    Best Regards,

    Pedro

Children
No Data