Post Go back to editing

ADSP-2148x E-pad question

Hello

I have just finished reading the EE- 352 Engineering note regarding E-pad packages and mounting techniques. One thing I am not clear of is you don't say whether or not you use thermal relief's or direct connects on the ground plane connecting via's. Obviously direct connection would give you better electrical connection and lower thermal resistance to the ground plane but would it alter the temperature profile needed for reflow ? ie which would be better from the point of view of manufacturability ?

regards

david

Parents
  • We apply paste to the pad before we place the part.

    I think hot air works better than an iron. If the small vias are not completely covered by the mask, you can see some outgassing which helps you know you are melting the solder.

    I should point out that I don't actually do any of this myself. I have skillful people. This means that this is the method I observe, but I could be a little off on the details. I know the hole size is correct since I lay out the PCBs.

    Al

Reply
  • We apply paste to the pad before we place the part.

    I think hot air works better than an iron. If the small vias are not completely covered by the mask, you can see some outgassing which helps you know you are melting the solder.

    I should point out that I don't actually do any of this myself. I have skillful people. This means that this is the method I observe, but I could be a little off on the details. I know the hole size is correct since I lay out the PCBs.

    Al

Children
No Data